ATOHPLCopen motion icon

FunctionClosedA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Converts string to integer using hexadecimal basis

Inputs

IN : STRING  String representing an integer in hexadecimal format

Outputs

Q : DINT     Integer represented by the string

Truth table (examples)

IN Q

''

0

'12'

18

'a0'

160

'A0zzz'

160

Remarks

The function is case insensitive. The result is 0 for an empty string. The conversion stops before the first invalid character. In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.

In ILClosed"Instruction list" This is a low-level language and resembles assembly, the input must be loaded in the current result before calling the function.

ST Language

Q := ATOH (IN);

FBD Language

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)

IL Language:

Op1: LDClosed"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     ATOH
     ST  Q

See also

HTOA

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen