AVERAGE / AVERAGELPLCopen motion icon

Function BlockClosedA function block groups an algorithm and a set of private data. It has inputs and outputs. - Calculates the average of signal samples.

Inputs

RUN : BOOL  Enabling command
XIN : REAL  Input signal
N   : DINT  Number of samples stored for average calculation - Cannot exceed 128

Outputs

XOUT : REAL Average of the stored samples (*)

(*) AVERAGEL has LREAL arguments.

Remarks

The average is calculated according to the number of stored samples, which can be less than N when the block is enabled. By default the number of samples is 128.

The "N" input (or the number of samples) is taken into account only when the RUN input is FALSE.


  • The "RUN" needs to be reset after a change in the number of samples. You should cycle the RUN input when you first call this function, this will clear the default.


  • In FFLD language, the input rung is the RUN command. The output rung keeps the state of the input rung.

ST Language

(* MyAve is a declared instance of AVERAGE function block *)
MyAve (RUN, XIN, N);
XOUT := MyAve.XOUT;

FBD Language

AverageFbd.gif (1455 octets)

FFLD Language

(* ENO has the same state as RUN *)
AverageLd.gif (1581 octets)

IL Language:

(* MyAve is a declared instance of AVERAGE function block *)
Op1: CAL MyAve (RUN, XIN, N)
     FFLD 
MyAve.XOUT
     ST  XOUT

See also

INTEGRAL   DERIVATE   LIM_ALRM   HYSTER  STACKINT

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen