eipWriteAttr
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Ethernet/IP explicit messaging - write single attribute.
This function block sends an explicit message (UCMM) to an Ethernet/IP adapter, for writing a single CIP
"Common Industrial Protocol "
The Common Industrial Protocol allows complete integration of control with information, multiple CIP Networks, and Internet technologies attribute.
Inputs
| Snd : BOOL | A rising edge |
| SrvIP : STRING | IP address of the server (adapter) such as configured in the "Ethernet/IP Scanner" configuration. |
| Class : UINT | Class identifier of the CIP object. |
| Inst : UINT | Instance identifier of the CIP object. |
| Attr : UINT | Identifier of the CIP attribute. |
| Size : UINT | Number of bytes to write. Cannot exceed 450 bytes. |
| Data : array of UINT | Buffer containing the data to write. |
Outputs
| Done : BOOL | This output is TRUE during one cycle when the exchange is finished, whatever the exchange succeeded or failed. Warning, this output can be TRUE just after the call to block when starting a new exchange in case of invalid parameters. |
| RcvSize : UINT | Actual size of the CIP attribute answered by the server. If this size if greater than the size of the DATA input array, it indicates that the value was truncated. |
| Err : UINT | Main error report. Can be one of the following values: 0 = no error 1 = invalid input arguments 2 = system is busy (see remarks) 3 = timeout waiting for the answer (the timeout value is 3 seconds 4 = UCMM error was returned by the server others = internal errors (reserved for technical support) |
| EmErr : UINT | in case of a UCMM error, this is the CIP general status error code. |
| EmErrExt : UINT | in case of a UCMM error, this is the CIP extended status error code. |
Remarks
The servers (adapters) accessed by this block must be configured in the "Ethernet/IP Scanner" fieldbus configuration.
Only one explicit message (read or write) can be sent at one time to the same server. If another message is pending then you will get the error report 3 (busy) after calling the block to start a new exchange.
Consider SerializeIn and SerializeOut functions for storing data to the write buffer.
Example
// used variables
// Inst_eipWriteAttr : eipWriteAttr ;
// bWrite : BOOL ; (* request for WRITE *)
// DataWrite : ARRAY [0 .. 15] OF USINT; (* written data *)
// uiSizeWrite : UINT := UINT#16 ; (* number of bytes to read *)
// Server identification and CIP things
#define SRVIP '192.168.33.21'
#define CLASSID UINT#100
#define INSTID_WRITE UINT#2
#define ATTRID UINT#3
/////////////////////////////////////////////////////////////////////////////////////////
// requested WRITE command
if bWrite then
Inst_eipWriteAttr (bWrite, SRVIP, CLASSID, INSTID_WRITE, ATTRID,
uiSizeWrite, DataWrite);
end_if;
// WRITE answer here ?
if Inst_eipWriteAttr.Done then
// check answer
if Inst_eipWriteAttr.Err = 0 then
printf ('WRITE ok');
else
printf ('WRITE Error %lu - (UCMM Error %lu, %lu)',
any_to_dint (Inst_eipWriteAttr.Err),
any_to_dint (Inst_eipWriteAttr.EmErr),
any_to_dint (Inst_eipWriteAttr.EmErrExt));
end_if;
// reset WRITE command and block input
Inst_eipWriteAttr (false, SRVIP, CLASSID, INSTID_WRITE, ATTRID,
uiSizeWrite, DataWrite);
bWrite := false;
end_if;
|
Copyright © 2018 Kollmorgen |
|