FBD comments

Comment text area can be entered anywhere in an FBDClosed"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks diagram.

Press the following button in the FBD toolbar to insert a new comment area.

In this mode, the mouse is used to insert comment text areas anywhere in the diagram.

Double-click on the comments area to enter or change the attached text. When selected, comment texts can be resized.


  • You can insert hyperlink on external files as shown below. Only TXT and BMP extensions are allowed. When the link is valid, the hyperlink is replaced with the file's content.

          

Figure 5-83: FBD Comments - Inserting Graphic

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen