Select FBD variables and instances

Press this button or press ESCAPE before any selection.

To select the name of the declared variable to be attached to a graphic symbol, you must be in "Selection" mode. Simply double-click on the tag-name gray area. The following types of object must be linked to valid symbols:

Block: If it is a function block, you must specify the name of a valid declared instance of the corresponding type. 

Variable: Must be attached to a declared variable. Alternatively, a variable box may contain the text of a valid constant expression. 

Label: Must have a name. The name must be unique within the diagram. 

Jump: Must have the same name as its destination label. 

Contact: Must be attached to a declared Boolean variable. 

Coil: Must be attached to a declared Boolean variable.

Symbols of variables and instances are selected using a variable list, that can be used as the variable editor. Simply enter a symbol or constant expression in the edit box and press OK. You can also select a name in the list of declared objects, or declare a new variable by pressing the "Create" button.

For more details, Select Variables and Instances

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen