FFLD Coils
Coils are basic graphic elements of the FFLD language. A coil is associated with a Boolean variable which is displayed above the graphic symbol. A coil performs a change of the associated variable according to the flow on its left-hand side.
Below are the six possible coil symbols:
| Coils | Description |
|---|---|
| boolVariable -( )- |
Normal: the associated variable is forced to the value of the flow on the left of the coil. |
| boolVariable -(/)- |
Negated: the associated variable is forced to the negation of the flow on the left of the coil. |
| boolVariable -(S)- |
Set: the associated variable is forced to TRUE if the flow on the left is TRUE. (no action if the flow is FALSE)
|
| boolVariable -(R)- |
Reset: the associated variable is forced to FALSE if the flow on the left is TRUE. (no action if the rung state is FALSE)
|
| boolVariable -(P)- |
Positive transition: the associated variable is forced to TRUE if the flow on the left changes from FALSE to TRUE(and forced to FALSE in all other cases) |
| boolVariable -(N)- |
Negative transition: the associated variable is forced to TRUE if the flow on the left changes from TRUE to FALSE(and forced to FALSE in all other cases) |
-
-
When a contact or coil is selected, you can press the Spacebar to change its type (normal, negated...)
When your application is running, you can select a contact and press the Spacebar to swap its value between TRUE and FALSE
-
-
Although coils are commonly put at the end, the rung can be continued after a coil. The flow is never changed by a coil symbol.
|
Copyright © 2018 Kollmorgen |
|