LIMIT
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Bounds an integer between low and high limits.
Inputs
IMIN : DINT Low bound
IN : DINT Inputvalue
IMAX : DINT High bound
Outputs
Q : DINT IMIN if IN < IMIN; IMAX if IN > IMAX; IN otherwise
Function diagram
Remarks
In FFLD language, the input rung (EN) enables the operation, and the output rung keeps
the state of the input rung. In IL
"Instruction list"
This is a low-level language and resembles assembly language, the first input must be loaded before the
function call. Other inputs are operands of the function, separated by a coma.
ST Language
Q := LIMIT (IMIN, IN, IMAX);
FBD Language
FFLD Language
(* The comparison is executed only if EN is TRUE *)
(* ENO has the same value as EN *)
IL Language:
See also
|
Copyright © 2018 Kollmorgen |
|