Registers

Below are the standard functions for managing 8 bit to 32 bit registers:

SHL shift left
SHR shift right
ROL rotation left
ROR rotation right

Below are advanced functions for register manipulation:

MBShift multibyte shift / rotate

The following functions enable bit to bit operations on a 8 bit to 32 bit integers:

AND_MASK Boolean AND
OR_MASK Boolean OR
XOR_MASK exclusive OR
NOT_MASK Boolean negation

The following functions enable to pack/unpack 8, 16 and 32 bit registers

LOBYTE Get the lowest byte of a word
HIBYTE Get the highest byte of a word
LOWORD Get the lowest word of a double word
HIWORD Get the highest word of a double word
MAKEWORD Pack bytes to a word
MAKEDWORD Pack words to a double word
PACK8 Pack bits in a byte
UNPACK8 Extract bits from a byte

The following functions provide bit access in 8 bit to 32 bit integers:

SETBIT Set a bit in a register
TESTBIT Test a bit of a register

The following functions have been deprecated. They are available for backwards compatibility only. The functions listed above should be used for all current and future development.

AND_WORD AND_BYTE
OR_WORD OR_BYTE
NOT_WORD NOT_BYTE
XOR_WORD
XOR_BYTE
ROLW RORW
ROLB RORB
SHLW SHRW
SHLB SHRB

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen