Jump to an SFC step
"Sequential function chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions charts to represent a link from a
transition to a step without actually drawing it. The jump is represented by an
arrow identified with the number of the target step.
-
-
To change the number of a step, transition or jump, select it and hit Ctrl+ENTER keys.
You cannot insert a jump to a transition as it may lead to a non explicit convergence of parallel branches (several steps leading to the same transition) and generally leads to mistakes due to a bad understanding of the chart.
All parallel convergences must be explicitly drawn.
|
Copyright © 2018 Kollmorgen |
|