Calling a sub-program

A sub-program is called by another program. Unlike function blocks, local variables of a sub-program are not instantiated, and thus you do not need to declare instances. A call to a sub-program processes the block algorithm using the specified input parameters. Output parameters can then be accessed.

ST Language

To call a sub-program in STClosed"Structured text" A high-level language that is block structured and syntactically resembles Pascal, you have to specify its name, followed by the input parameters written between parentheses and separated by comas. To have access to an output parameter, use the name of the sub-program followed by a dot '.' and the name of the wished parameter:

MySubProg (i1, i2); (* calls the sub-program *)
Res1 := MySubProg.Q1;
Res2 := MySubProg.Q2;

Alternatively, if a sub-program has one and only one output parameter, it can be called as a function in ST language:

Res := MySubProg (i1, i2);

FBD and FFLD Languages

To call a sub-program in FBDClosed"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks or FFLD languages, you just need to insert the block in the diagram and to connect its inputs and outputs.

IL Language

To call a sub-program in ILClosed"Instruction list" This is a low-level language and resembles assembly language, you must use the CAL instruction with the name of the sub-program, followed by the input parameters written between parentheses and separated by comas. Alternatively the CALC, CALCN or CALNC conditional instructions can be used:

CAL    Calls the sub-program
CALC   Calls the sub-program if the current result is TRUE
CALNC  Calls the sub-program if the current result is FALSE
CALCN  same as CALNC

Here is an example:

Op1: CAL  MySubProg (i1, i2)
FFLD MySubProg.Q1
ST Res1
FFLD MySubProg.Q2
ST Res2

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen