Working with Variables

All variables used in programs must be first declared in the variable editor. Each variable belongs to a group and must be identified by a unique name within its group.

Groups

A group is a set of variables. A group either refers to a physical class of variables, or identifies the variables local to a program or user-defined function block. Below are the possible groups:

Groups Description
GLOBAL Internal variables known by all programs
RETAIN Non volatile internal variables known by all programs
%I... Channels of an input board - variables with same data type linked to a physical input device
%Q... Channels of an output board - variables with same data type linked to a physical output device
PROGRAMxxx All internal variables local to a program
(the name of the group is the name of the program)
UDFBxxx All internal variables local to a User-Defined Function BlockClosedA function block groups an algorithm and a set of private data. It has inputs and outputs. plus its IN and OUT parameters
(the name of the group is the name of the program)

Data type and dimension

Each variable must have a valid data type. It can be either a basic data type or a function block. In the later case, the variable is an instance of the function block. Physical I/Os must have a basic data type. Instances of function blocks can refer either to a standard block, or to a User Defined FunctionClosedA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Block.

If the selected data type is STRING, you must specify a maximum length. This cannot exceed 255 characters.

Refer to the list of available data types for more information. Refer to the section describing function blocks for further information about how to use a function instance.

Additionally, you can specify dimension(s) for an internal variable, in order to declare an array.

Naming a variable

A variable must be identified by a unique name within its parent group. The variable name cannot be a reserved keyword of the programming languages and cannot have the same name as a standard function or function block (for a list, click here...). A variable must not have the same name as a program or a user-defined function block.

The name of a variable must begin by a letter or an underscore ("_") mark, followed by letters, digits or underscore marks. It is not allowed to put two consecutive underscores within a variable name. Naming is case-insensitive. Two names with different cases are considered as the same.

%IX 1 byte input - BOOL or SINT
%QX 1 byte output - BOOL or SINT
%IW 2 bytes input - INT
%QW 2 bytes output - INT
%ID 4 bytes input - DINT or REAL
%QD 4 bytes input - DINT or REAL
%IL 8 bytes input - LINT or LEAL
%QL 8 bytes output - LINT or LEAL
%IS STRING input
%QS STRING output

Attributes of a variable

Physical I/Os are marked as either "Input" or "Output". Each internal variable can be configured as Read/Write or Read Only. Read Only variables can be mapped to Outputs, but not to Inputs. This is because Inputs can change state and a Read Only variable would not be able to change its value to match the input state.

Parameters of User-Defined Function Blocks are marked as either INor OUT.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen