WHILE DO END_WHILE
Syntax
WHILE <BOOL expression> DO
<statements>
END_WHILE ;
Remarks
The statements between "DO" and "END_WHILE" are executed while the Boolean expression is TRUE. The condition is evaluated beforethe statements are executed. If the condition is FALSE when WHILE is first reached, statements are never executed.
-
-
Loop instructions can lead to infinite loops that block the target cycle. Never test the state of an input in the condition as the input will not be refreshed before the next cycle.
ST Language
iPos := 0;
WHILE iPos < iMax DO
MyArray[iPos] := 0;
iNbCleared := iNbCleared + 1;
END_WHILE;
FBD Language
Not available
FFLD Language
Not available
IL Language
Not available
See also
|
Copyright © 2018 Kollmorgen |
|