Known Issues

Defect Description
BZ-10275 PxMM controller bus time not synchronized with DC master time
BZ-9975 KAS IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger crashes in the Workbench Performance Servo Tuner Window
BZ-9928 ESI file list is not updated when good and bad ESI files are added at the same time
BZ-9848 KAS IDE broken if Windows user name contains non-ascii characters
BZ-9835 Non-ASCII characters in projects not handled properly in the KAS IDE
BZ-9834 Import/export from/to non-ascii file names does not work correctly
BZ-9832 Cannot add libraries (.KAL files) with non-ASCII file names
BZ-9496 AKD-N firmware download fails if 4x drives are selected
BZ-9359 PDO objects not defined in the object dictionary (or 24bit size) will not work properly with MLSmpXxxxx(...) functions
BZ-8659 PLCopenClosedA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML move blending with jerkClosedIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time. If the blending move is commanded with an unreachable velocity, the move may abruptly decelerate to the final position within one sample, exceeding the specified deceleration rate.
BZ-8654 E21 when KAS IDE running O-Scope is disconnected
BZ-8645 Adding ESI File After Scanning Results in No Selected PDOs
BZ-8644 PLCopen S-Curve move may not reach target with small JerkClosedIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time
BZ-8643 EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs scan fails after a AKD drive firmware download failure with a wrong EtherCAT topology
BZ-8636 Recovered projects don’t recover imported libraries (.kal files)
BZ-8633 When a crash report fails due to error (ex - timeout, connection failure, …) report is lost. User cannot resend.
BZ-8608 KAS IDE views do not scale if Windows text scaling is > 100%
BZ-8605 MLInitTrig does not configure the AKD Capture engine correctly for a negative edge trigger.
BZ-8588 ECAT network restore fails to recover from drive FW download failure.
BZ-8508 PDOs need padding to meet byte boundary requirement. The IDE PDO Editor does not automatically pad PDOs on non-byte boundaries. The problem can be avoided by manually adding dummy objects to pad the PDO size to line-up on byte boundaries. For more details, see the article on KDN.
BZ-8504 KL3314 Operation. Temperature values are not calibrated properly to the thermocouple. To work-around the problem, use ECATWriteData to setup the control word (16xE0) and send value (16x2006) to Register R32 and a second ECATWriteData to write zero (0) to the control word to set up the continual output of the temperature.
BZ-8482 ModbusClosedModBus is a serial communications protocol and is now the most commonly available means of connecting industrial electronic devices. ModBus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems. Versions of the ModBus protocol exist for serial port and Ethernet (it is widely used with TCP/IP over Ethernet) renumber address does not work with String variables. In the FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Editor Modbus configurator, if you right click input registers and choose the renumber address option, it will make the addresses overlap.
BZ-8242 Missed cycles while doing file operations
BZ-8212 Modified cam file is not downloaded when forcing an Online Change.
BZ-8138 WebBrowser component not working for TxB panels
BZ-8132 K-Bus slices analog inputs Offset parameter does not work
BZ-7985 IDE disconnects from the controller after several days
BZ-7759 Breakpoint with For(…) loop, increases VM load significantly
BZ-7728 IDE animation with non-matching project versions
BZ-6240 IDE always reports the project has been modified

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen