AKD Setup Wizard

The Setup Wizard contains step-by-step instructions for configuring a drive for the first time and generating a simple test motion. You can access the Setup Wizard from the Drive Overview screen, or by right clicking on the drive name.

  1. Access the Setup Wizard by double-clicking on the drive name in the project view.
  2. Enable Online Configuration mode from the toolbar, by pressing the “Toggle Online Configuration Mode” button.
  3. After the drive is connected, you can press the Setup Wizard... button in the Drive Overview screen


The Setup Wizard is useful during the initial setup. The wizard confirms your connection with the drive and leads you through a series of steps to quickly get your drive up and running. With plug and play feedback devices, several steps are skipped (feedback, brake) because the drive automatically configures these settings. For all systems, you can select the units you want to use, configure your operation mode, tune the system, and perform some simple jog moves within the wizard. After you are comfortable with the basic system setup, you can save your settings to the drive and exit the wizard.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen