Plugging Probes, Mapping Variables
Three types of variables can be mapped:
- Pipe Block variable
- IEC
"International Electrotechnical Commission"
IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 variable, which is any other variable. - PLCOpen axis values.
You can connect a probe to a variable in one of the following ways:
- from the Softscope, see Mapping a Variable to the Oscilloscope
- from the Dictionary, see Plugging a probe from the Dictionary
- from the Pipe Network, Plugging a probe from the Pipe Network