REC.TRIGMASK
Description
This keyword sets the mask associated with a Scope trigger of type Bitmask (REC.TRIGTYPE 5). When the trigger is armed, it does not activate until the trigger parameter (REC.TRIGPARAM) reaches a value such that if masked with REC.TRIGMASK, the resulting value becomes equal to REC.TRIGVAL .
Examples
Code
When REC.TRIGTYPE = 5, REC.TRIGPARAM is DIN.STATES, and REC.TRIGVAL = 3, the trigger will not activate till both DIN1 and DIN2 are high.
-->REC.TRIGMASK 3
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 0xFFFFFFFF |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.