MOTOR.IDDATAVALID
Description
MOTOR.IDDATAVALID reports the status of the motor memory status.
The valid values for this keyword are the following:
|
Value |
Description |
|---|---|
|
0 |
Error in identification |
|
1 |
Success in identification |
|
2 |
Identification in process |
|
3 |
Identification not started yet |
|
4 |
Success recognizing feedback, but failed to varify OEM |
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-02-00-000 |
Related Topics