MOTOR.LDLL
Description
This parameter is the motor line to line direct axis inductance. It is supported for the IPM motor type (MOTOR.TYPE = 6).
-
-
This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.
General Information
|
Type |
NV Parameter |
|
Units |
mH |
|
Range |
1 to 2^31 |
|
Default Value |
17.000 |
|
Data Type |
Float |
|
Start Version |
M_01-11-00-000 |
Related Topics