MLCNVConnectEx
Description
Connect a converter Pipe Block to the specified axis. This function connects the output of a pipe to an axis data other than the control position. With this function, several converter Pipe Blocks can connect to the same axis and acts on different data.
Normally a Converter block sends position values to an Axis. However, some cases exist that require additional information such as torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist feed-forward
This describes an element or pathway within a control system which passes a controlling signal from a source in the control system's external environment, often a command signal from an external operator, to a load elsewhere in its external environment (IDN 3056) that needs to be provided by a second converter.
-
-
This FB does not work when you choose to simulate the device. In such a case, the FB continuously generates error messages displayed in the Controller log window.
-
-
Need to add 16#8000 to desired IDN number for ValueID input. 8000 in hexadecimal signals a vendor-specific IDN value.
Arguments
Input
| BlockID | Description | ID number of an initiated Converter object |
| Data type | DINT | |
| Range | [-2147483648, 2147483648] | |
| Unit | N/A | |
| Default | — | |
| AxisID | Description | ID number of an initiated Axis object |
| Data type | DINT | |
| Range | [-2147483648, 2147483648] | |
| Unit | N/A | |
| Default | — | |
| ValueID | Description |
Specify the following constant:
If the Analog Output is mapped to a PLC See the TIP below for more information. |
| Data type | DINT | |
| Range | [-2147483648, 2147483648] | |
| Unit | N/A | |
| Default | — | |
| ValueInfo | Description |
This value is ignored and must be set to zero |
| Data type | DINT | |
| Range | [-2147483648, 2147483648] | |
| Unit | N/A | |
| Default | — |
-
-
The PDO values will be overwritten by Mapped PLC variables including a possible link to the mapping of variables or the section on MLParamWrite() warning indicating that the function block write of Analog output will be overwritten by the MLCnvConnectEx function.
- A PLC variable mapped to Analog Output takes precedence
In arithmetic and algebra, when a number or expression is both preceded and followed by a binary operation, a rule is required for which operation should be applied first. From the earliest use of mathematical notation, multiplication took precedence over addition, whichever side of a number it appeared on. Thus 3 + 4 × 5 = 5 × 4 + 3 = 23.
To change the order of operations, we use parentheses (). Thus, if we want to force addition to precede multiplication, we write (3 + 4) × 5 = 35. - If MLCNVConnect assigns a Pipe output to Analog Output it will take precedence over a DriveParamWrite function call.
- DriveParamWrite will modify the Analog Output but get overwritten by the higher precedent options if they are present.
- A PLC variable mapped to Analog Output takes precedence
Output
|
Default (.Q) |
Description | Returns TRUE if the converter is connected to the Axis object See more details here. |
| Data type | BOOL | |
| Unit | N/A |
Return Type
BOOL
Related Functions
Example
Structured Text
//Connect a converter Pipe Block named “CNV1” to the pipe block named AXIS1, And send feed-forward (EC_ADDITIVE_TORQUE_VALUE) to the drive
MLCNVConnectEx( PipeNetwork.CNV1, PipeNetwork.AXIS1, EC_ADDITIVE_TORQUE_VALUE, 0 );
Ladder Diagram
Function Block Diagram
[Top]