MC_MoveDirRel

Description
MC_MoveDirRel commands a movement of an axes group to a relative position in the specified coordinate system without taking care of how (on which path) the target position is reached.
-
-
- An error is returned if the group is in the GroupDisabled state.
- This function block does not have its own Acceleration, Deceleration, Velocity, and Jerk
In physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time arguments. These are set using MC_AxisSetDefaults. - The maximum number of axes is set by the MaxNumberOfAxes input set in the MC_CreateAxesGrp function block.
- S-Curve motion is not currently supported. The Jerk input is currently ignored. S-Curve motion and the Jerk argument will be supported in a future release. .
When all motion has completed successfully, the state of the axes group goes to GroupStandby.
Related Functions
MC_MoveDirAbs, MC_ErrorDescription
Coordinated Motion, the top-level topic for Coordinated Motion.
Arguments
For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules
Input
| Execute | Description |
On the rising edge |
| Data type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| AxesGroup | Description | Reference to an axes group |
| Data type | AXES_GROUP_REF | |
| Range | — | |
| Unit | N/A | |
| Default | — | |
| Distance[ ] | Description | An array containing the distance for each axis in the group. |
| Data type | LREAL | |
| Range | [0, Number of axes in group - 1] | |
| Unit | N/A | |
| Default | — | |
| CoordSystem | Description |
The coordinate system used when commanding the direct relative move. Currently, only the ACS coordinate system is supported. See Coordinate Systems to learn more. |
| Data type | SINT | |
| Range |
|
|
| Unit | N/A | |
| Default | — | |
| BufferMode | Description |
Defines the chronological sequence of the function block relative to the previous block. See the table in Buffer Modes |
| Data type |
SINT MC_BUFFER_MODE_ABORTING = 0 = Abort |
|
| Range | — | |
| Unit | N/A | |
| Default | — |
Output
| Done | Description |
If True, then the command completed successfully. |
| Data type | BOOL | |
| Busy | Description |
If True, then the function block is executing. . |
| Data type | BOOL | |
| Active | Description |
If True, then the function block is controlling motion. |
| Data type | BOOL | |
| CommandAborted | Description |
If True, command was aborted by another function block. |
| Data type | BOOL | |
| Error | Description | If True, an error has occurred. |
| Data type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE. See table in PLCopen Function Block ErrorID Output. |
| Data type | INT |
Example
Structure Text
Inst_MC_MoveDirRel( ExecuteMove, Group1_Ref, DistanceList, MC_COORDINATE_SYSTEM_ACS, MC_BUFFER_MODE_ABORTING );
IL
BEGIN_IL
"Instruction list"
This is a low-level language and resembles assembly
CAL Inst_MC_MoveDirRel( ExecuteMove, Group1_Ref, DistanceList, MC_COORDINATE_SYSTEM_ACS, MC_BUFFER_MODE_ABORTING )
END_IL
Function Block Diagram
Ladder Diagram
[Top]