MC_InitAxesGrp

Description
MC_InitAxesGrp initializes the kinematic limits for the axis group. During a move, the motion engine verifies that the limits are not exceeded.
-
-
The function block returns an error if the group state is not GroupStandby or GroupDisabled.
Related Function Blocks
MC_CreateAxesGrp, MC_ErrorDescription
Coordinated Motion, the top-level topic for Coordinated Motion.
Arguments
Inputs
| Execute | Description | On the rising edge |
| Data type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| AxesGroup | Description | The axis group to be initialized |
| Data type | AXIS_GROUP_REF | |
| Range | N/A | |
| Unit | N/A | |
| Default | — | |
| VelocityLimit | Description | Velocity limit |
| Data type | LREAL | |
| Range | 0 < Velocity < ( 20 * Acceleration ) and 0 < Velocity < ( 20 * Deceleration) See Limitations on Acceleration and Jerk for more information. |
|
| Unit | user units per second | |
| Default | — | |
| AccelerationLimit | Description | Acceleration limit |
| Data type | LREAL | |
| Range |
0 < Velocity < ( 20 * Acceleration ) |
|
| Unit | user units per second2 | |
| Default | — | |
| DecelerationLimit | Description | Deceleration limit |
| Data type | LREAL | |
| Range | 0 < Velocity < ( 20 * Deceleration) See Limitations on Acceleration and Jerk for more information. |
|
| Unit | User units per second2 | |
| Default | — | |
| JerkLimit | Description | Jerk limit |
| Data type | LREAL | |
| Range | ( Velocity / 20 ) < Acceleration < ( 2 * Jerk ) and ( Velocity / 20 ) < Deceleration < ( 2 * Jerk ) See Limitations on Acceleration and Jerk for more information. |
|
| Unit | User units per second3 | |
| Default |
Outputs
| Done | Description |
If True, then the command completed successfully. |
| Data type | BOOL | |
| Error | Description |
If True, then an error has occurred. |
| Data type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE. See the table in PLCopen Function Block ErrorID Output |
| Data type | INT |
Example
Structured Text
(* Inst_MC_InitAxesGrpST example *)
Inst_MC_InitAxesGrp( initAxesGrp, grp, velLim, accelLim, decelLim, jerkLim );
IL
BEGIN_IL
"Instruction list"
This is a low-level language and resembles assembly
CAL Inst_MC_InitAxesGrp( initAxesGrp, grp, velLim, accelLim, decelLim, jerkLim )
END_IL
FBD
FFLD
[Top]