MC_UngroupAllAxes

Description
MC_UngroupAllAxes removes all axes from an axes group. This function block can be issued in the group states: (GroupDisabled, GroupStandby, or GroupErrorStop). The axes group state will be changed to GroupDisabled upon successful completion. This function block does not cause any motion.
-
-
MC_UngroupAllAxes will fail if the group is in any state other than GroupStandby or GroupDisabled.
Refer to Group State Diagrams for details.
Figure 7-163: MC_UngroupAllAxes
Related Functions
MC_AddAxisToGrp, MC_RemAxisFromGrp, MC_ErrorDescription
Coordinated Motion, the top-level topic for Coordinated Motion.
-
- This function block starts a motion-related action and therefore stores data for calculations and error checking. Please see Calling Function Blocks Multiple Times in the Same Cycle if you are using a dual-core controller.
Arguments
Input
| Execute | Description | On the rising edge |
| Data type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| AxesGroupRef | Description | The axis group from which to remove all axes |
| Data type | AXIS_GROUP_REF | |
| Range | N/A | |
| Unit | N/A | |
| Default | — |
Output
| Done | Description | If True, then the command completed successfully. |
| Data type | BOOL | |
| Error | Description | If True, an error has occurred |
| Data type | BOOL | |
| ErrorID | Description | Indicates the error identifier if 'Error' output is set to TRUE. See the table in PLCopen Function Block ErrorID Output. |
| Data type | INT |
Examples
ST
Inst_MC_UngroupAllAxes( ExecuteUngroup, Group1_Ref );
IL
BEGIN_IL
"Instruction list"
This is a low-level language and resembles assembly
CAL Inst_MC_UngroupAllAxes( ExecuteUngroup, Group1_Ref )
END_IL
FBD
FFLD
[Top]