TcpSend
Description
This function block sends characters over a socket. It is possible that the number of characters actually sent is less than the number expected. In that case, you will need to use TcpSend again to send the pending characters.
-
- It is possible that the socket becomes invalid if an error occurs in the TCP connection after this function block is called. You must use the TcpIsValid function block after TcpSend. If the socket is no longer valid then you must close it by using the TcpClose function block.
Figure 7-215: The TcpSend function block
Related Functions
TcpAccept, TcpBinReceive, TcpBinSend, TcpClose, TcpConnect, TcpIsConnected, TcpIsValid, TcpListen, TcpReceive
Arguments
Input
| Execute | Description | On the rising edge |
| Data Type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| ID | Description | The ID of the client socket. |
| Data Type | UDINT | |
| Range | N/A | |
| Unit | N/A | |
| Default | — | |
| NbChar | Description | The number of characters to send. |
| Data Type | DINT | |
| Range | N/A | |
| Unit | N/A | |
| Default | — | |
| Data | Description | The IP Address of the remote server. |
| Data Type | STRING | |
| Range | N/A | |
| Unit | N/A | |
| Default | — |
Output
| Done | Description | If TRUE, then the command completed successfully |
| Data Type | BOOL | |
| Error | Description | If TRUE, an error has occurred |
| Data Type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE. See the table in Search IndexFile and TCP/IP Function Block ErrorID Output |
| Data Type | DINT | |
| NbSent | Description | The number of characters actually sent. |
| Data Type | DINT |
Example
Structured Text
(* TcpSend example *)
CASE StepCounter OF
0:
Inst_TcpSend(TRUE, MySocketID, 5, 'Hello');
StepCounter := StepCounter + 1;
1:
Inst_TcpSend(TRUE, MySocketID, 5, 'Hello');
IF Inst_TcpSend.Done THEN
BytesSent := Inst_TcpSend.NbSent;
Inst_TcpSend(FALSE, 0, 0, '');
StepCounter := StepCounter + 1;
END_IF;
END_CASE;