AXIS#.HOME.MODE
Description
AXIS#.HOME.MODE specifies the homing procedure of the drive. The homing modes available in the drive are summarized in the following table. See HomingThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position for a detailed description of each mode:
Mode | Description |
---|---|
0 |
Current position |
1 |
Find limit switch |
2 |
Find limit switch then find zero angle |
3 |
Find limit switch then find index |
4 |
Find home switch |
5 |
Find home switch then find zero angle |
6 |
Find home switch then find index |
7 |
Find zero angle |
8 |
Find end stop |
9 |
Find end stop then find zero angle |
10 |
Find end stop then find index |
11 |
Find index signal, without any precondition |
12 |
Find home switch, including end stop detection |
13 | Absolute feedback |
14 | reserved |
15 | Find next feedback zero position |
16 | Find home switch using dual edges |
19 | Gantry Homing: Use Master Settings |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
Type |
Read/Write |
Units |
N/A |
Range |
0 to 15 |
Default Value |
0 |
Data Type |
Integer |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.HOME.MODE | 0x5008 | 0x2 | UINT | - | - | RW | False |
AXIS2.HOME.MODE | 0x5108 | 0x2 | UINT | - | - | RW | False |
Related Topics
Homing