AXIS#.HOME.P

Description

AXIS#.HOME.P is the position given to the home point once it is found.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float

See Also

AXIS#.HOME.MODE

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Related Topics

Homing