AXIS#.UNIT.LABEL
Description
If you define a custom position unit with AXIS#.UNIT.PIN and AXIS#.UNIT.POUT , then you can give this unit a descriptive name. You can name the unit anything you wish, as long as the name is limited to 16 characters. The label used for velocity and acceleration are in terms of this descriptive name.
This parameter is descriptive only and does not influence drive internal functions in any way.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
Maximum 16 characters |
Default Value |
Custom Units |
Data Type |
String |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics
Selecting Units for Your Application