AXIS#.VL.FF

Description

This parameter displays the velocity loop overall feedforward value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: RPMClosed"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

0 to AXIS#.VL.LIMITP

Default Value

0

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Related Topics

Velocity Loop

AXIS#.VL.KVFF