REC.TRIGPARAM
Description
REC.TRIGPARAM sets the parameter which the recorder uses to trigger the capture.
This parameter is not used when REC.TRIGTYPE is 0 (Immediate) or 1 (On Next Command).
Input values are:
- One of the set drive parameters list that can be set as a trigger. The available parameters for trigger are: AXIS#.PL.ERR , AXIS#.PL.CMD , AXIS#.PL.FB , AXIS#.VL.CMD, AXIS#.VL.FB , AXIS#.IL.CMD , and AXIS#.IL.FB .
- Internal value or variable of the drive.
Examples
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
AXIS1.IL.FB |
|
Data Type |
String |
|
See Also |
|
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.