BODE.FREQ
Description
BODE.FREQ sets the frequency of the sine excitation source in Hz. The sine excitation source is used to take frequency response measurements of a system.
Example
Setting up a sine excitation source of 0.2 A at 50 Hz:
-->BODE.INJECTPOINT 1
-->BODE.IAMP 0.2
-->BODE.FREQ 50.0
-->BODE.MODE 2
General Information
|
Type |
R/W Parameter |
|
Units |
Hz |
|
Range |
0 to 8,000 Hz |
|
Default Value |
0 Hz |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
Related Topics
Using the Performance Servo Tuner
Using the Performance Servo Tuner: Advanced