CS.STATE
Description
CS.STATE returns the internal state machine value of the controlled stop.
0 = controlled stop is not occurring.
1 = controlled stop is occurring
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3441h/0 |
M_01-00-00-000 |
Related Topics