DRV.HWENABLE

Description

Status of the Hardware Enable.

0 - not enabled

1 - enabled

Notes: This parameter reflects the status of the hardware enable only, not if the status of the power stage. The status of the power stage enable is determined by DRV.ACTIVE.

General Information

Type

R/O

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

Start Version

M_01-18-00-004

Related Topics

DRV.DISSOURCES | DRV.ACTIVE