MOTOR.VOLTRATED
Description
This parameter configures the drive for the induction motor's rated voltage as indicated on the nameplate.
MOTOR.VOLTRATED is used to calculate the constant Volts per Hertz characteristics of the drive and motor.
-
-
If MOTOR.AUTOSET = 1 and FB1.MEMVER > 0.01, this parameter will be automatically configured for Kollmorgen motors.
General Information
|
Type |
NV Parameter |
|
Units |
V |
|
Range |
50 to 1,000 V |
|
Default Value |
230 V |
|
Data Type |
U16 |
|
See Also |
|
|
Start Version |
M_01-03-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3457h/2 |
M_01-03-00-000 |
Related Topics