REC.RECPRMLIST

Description

This command returns the list of recordable parameters. You can use a recordable parameter as an input to any of the recording channels.

Note that an internal address or a registered variable can be used as input to any of the channels in addition to the list.

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REC.CH1 to REC.CH6

Start Version

M_01-00-00-000

Related Topics

Scope