REC.CH1 to REC.CH6

Description

REC.CHx specifies the recording channels.

There are 3 options to set the recording channels values:

  • Set 0, CLR, or CLEAR. This setting clears the recording channel.
  • Set one of the recordable commands. The list of recordable commands can be obtain by executing REC.RECPRMLIST.
  • Set an internal value or variable of the drive (same as for DRV.MEMADDR input).

General Information

Type

R/W Parameter

Units

N/A

Range

N/A

Default Value

CH1 = ILClosed"Instruction list" This is a low-level language and resembles assembly.FB

CH2 = IL.CMD

CH3 = VL.FB

CH4 = Empty

CH5 = Empty

CH6 = Empty

Default Value

CH1 = STRINGS.I2TVALUE

CH2 = STRINGS.IVALUE

CH3 = STRINGS.STOSTATE

Data Type

String

See Also

REC.TRIG

Start Version

M_01-00-00-000

Related Topics

Scope