REC.TRIGTYPE

Description

REC.TRIGTYPE sets the type of trigger.

Input values are as follows:

Value

Description

0

Recording starts immediately

1

Recording starts on the next command executed through the TCP/IP. The trigger location in the buffer is set according to REC.TRIGPOS.

2

Recording starts per the values of REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE, and REC.TRIGPOS.

3

Recording starts when the value of REC.TRIGPARAM is 0 for REC.TRIGSLOPE = 0 or 1 for REC.TRIGSLOPE = 1

General Information

Type

R/W Parameter

Units

0 = immediate

1 = command

2 = parameter

3 = boolean

Range

0 to 3

Default Value

0

Data Type

Integer

See Also

REC.TRIG , REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE REC.TRIGPOS

Start Version

M_01-00-00-000

Related Topics

Scope