REC.TRIGVAL

Description

REC.TRIGVAL is the value that must be met by REC.TRIGPARAM for the trigger to occur. The units of this parameter are set according to the units of REC.TRIGPARAM.

General Information

Type

R/W Parameter

Units

The units of the parameter are chosen according to the unit type.

Range

-9223372036854775.808 to 9223372036854775.807

Default Value

0

Data Type

Integer

See Also

REC.TRIG , REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE, REC.TRIGPOS

Start Version

M_01-00-00-000

Related Topics

Scope