REGEN.POWERFILTERED
Description
This parameter returns a filtered value of REGEN.POWER. A single order lowpass of 1/REGEN.TEXT Hz is applied to generate REGEN.POWERFILTERED.
If REGEN.POWERFILTERED exceeds the value of REGEN.WATTEXT, Fault 521 (Regen overpower) will be generated.
This keyword may be recorded in the scope screen for analysis.
Example
REGEN.TEXT = 10 (seconds)
Lowpass Filter Frequence = 1/10 seconds = 0.1 Hz
REGEN.POWERFILTERED = REGEN.POWER * 0.1Hz lowpass
General Information
|
Type |
R/O parameter |
|
Units |
Watt |
|
Range |
0 to REGEN.WATTEXT |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-07-01-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3417h/0 |
M_01-00-00-000 |
Related Topics