WS.CHECKT
Description
This parameter sets the amount of time a commutation error must be present before an error is thrown. Commutation monitoring is disabled when this parameter is set to 0.
General Information
|
Type |
R/W Parameter |
|
Units |
ms |
|
Range |
0 to 10,000 |
|
Default Value |
N/A |
|
Data Type |
U16 |
|
Start Version |
M_01-06-03-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5352h/0 |
M_01-06-03-000 |
Related Topics