AIN.OFFSET
Description
AIN.OFFSET sets the analog offset, which is added to the analog input command to the drive. This value compensates for the analog input signal (AIN.VALUE ) offset or drift.
General Information
Type |
NV Parameter |
Units |
V |
Range |
–10 to +10 V |
Default Value |
0 V |
Data Type |
Float |
See Also |
|
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNetSynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Index/Subindex |
Object Start Version |
|
---|---|---|
5003h/0 |
M_01-00-00-000 |
Related Topics
Block Diagram for Position/Velocity Loop (pg 1)