AIN.VALUE

Description

AIN.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).

General Information

Type

R/O Parameter

Units

V

Range

-12.5 to +12.5 V

Default Value

N/A

Data Type

Float

Start Version

M_01-00-00-000

Variants Supported

*In SynqNetClosedSynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3470h/4

3509h/0

M_01-00-00-000

Related Topics

Analog Input

AIN.ZERO

AIN.OFFSET

Block Diagram for Position/Velocity Loop (pg 1)