Function BlockFileReadBinDataPLCopen motion icon

Description

This function block reads binary data from a file. FileReadBinData stops reading from the file if it fills the passed FrameClosedIn networking dialect, a message is called a frame array, reads FrameSize bytes, or encounters the end of file, whichever comes first.

After a successful call to FileReadBinData, one may use SerializeIn to extract variable data from the binary data read from a file.

Figure 7-209: The FileReadBinData Function Block

Related Functions

FileClose, FileEOF, FileOpenA, FileOpenR, FileOpenW, FileReadLine, FileSeek, FileWriteBinData, FileWriteLine, SerializeIn

See also: File Management

Arguments

Input

Execute Description On the rising edgeClosedA rising edge is the transition of a digital signal from low to high. It is also called positive edge read the size of a file.
  Data Type BOOL
  Range 0, 1
  Unit N/A
  Default —
ID Description ID of the open file.
  Data Type UDINT
  Range N/A
  Unit N/A
  Default —
Frame Description Where the binary data will be stored
  Data Type USINT[]
  Range N/A
  Unit N/A
  Default —
FrameSize Description Number of bytes to store in the Frame array.
  Data Type DINT
  Range N/A
  Unit N/A
  Default —

Output

Done Description If TRUE, then the command completed successfully
  Data Type BOOL
Error Description If TRUE, an error has occurred
  Data Type BOOL
ErrorID Description Indicates the error if Error output is set to TRUE. See the table in Search IndexFile and TCP/IP Function Block ErrorID Output
  Data Type DINT
NbRead Description The number of bytes read from the file.
  Data Type STRING

Example

Structured Text

(* FileReadBinData example *)
CASE StepCounter OF
0:
  Inst_FileReadBinData(TRUE, MyInputFileID, InputFrame, 128);
  StepCounter := StepCounter + 1;
1:
  Inst_FileReadBinData(TRUE, MyInputFileID, InputFrame, 128);
  IF Inst_FileReadBinData.Done THEN
     BytesRead := Inst_FileReadBinData.NbRead;
     Inst_FileReadBinData(FALSE, 0, InputFrame, 0);
     StepCounter := StepCounter + 1;
  END_IF;
END_CASE;