Search IndexFile and TCP/IP Function Block ErrorID Output
Following is the list of possible errors that could be returned at the ErrorID ourput of the File Tools Function Blocks and Search IndexTCP/IP Function Blocks.
File Function Block Errors
| 16000 |
Error opening file. |
| 16001 |
All file handles used. |
| 16002 |
File ID is invalid. |
| 16003 |
File ID has been closed. |
| 16004 |
Error in file stream. |
| 16005 |
End of file encountered. |
| 16006 |
Internal file FB error. |
| 16007 |
Unknown file error. |
| 16008 |
No such file or directory. |
| 16009 |
Bad file descriptor. |
| 16010 |
File already exists. |
| 16011 |
Too many open files in the system. |
| 16012 |
Text file is busy. |
| 16013 |
File is too large. |
| 16014 |
File system is read only. |
| 16015 |
File locking deadlock. |
| 16016 |
Filename is too long. |
| 16017 |
File positioning error. |
| 16018 |
Bad or corrupted file system detected . |
TCP/IP Function Block Errors
| 16100 |
Connection error. |
| 16101 |
TCP ID has been closed. |
| 16102 |
All PLC TCP handles used. |
| 16103 |
TCP ID is invalid. |
| 16104 |
Failed to allocate TCP/IP socket. |
| 16105 |
TCP operation internal error. |