Search IndexTCP/IP Function Blocks
This section documents function blocks that are used to communicate via TCP/IP.
| Function Block | Description |
|---|---|
| TcpAccept | Performs the accept operation. |
| TcpBinReceive | Receives characters over a socket connection. |
| TcpBinSend | Sends characters over a socket. |
| TcpClose | Closes and releases a socket. |
| TcpConnect | Creates a new socket and performs the connect operation. |
| TcpIsConnected | Tests if a client socket is connected. |
| TcpIsValid | Tests if a socket is valid. |
| TcpListen | Creates a new socket by performing the bind and listen operations. |
| TcpReceive | Receives characters over a socket connection. |
| TcpSend | Sends characters over a socket. |