Function BlockTcpClosePLCopen motion icon

Description

This function block closes and releases a socket. You are responsible for closing any socket created by the TcpListen, TcpAccept, or TcpConnect function blocks, even if they have become invalid.

Figure 7-219: The TcpClose function block

Related Functions

TcpAccept, TcpBinReceive, TcpBinSend, TcpConnect, TcpIsConnected, TcpIsValid, TcpListen, TcpReceive, TcpSend

Arguments

Input

Execute Description On the rising edgeClosedA rising edge is the transition of a digital signal from low to high. It is also called positive edge close a socket.
  Data Type BOOL
  Range 0, 1
  Unit N/A
  Default —
ID Description The ID of the client socket
  Data Type UDINT
  Range N/A
  Unit N/A
  Default —

Output

Done Description If TRUE, then the command completed successfully
  Data Type BOOL
Error Description If TRUE, an error has occurred
  Data Type BOOL
ErrorID Description Indicates the error if Error output is set to TRUE. See the table in Search IndexFile and TCP/IP Function Block ErrorID Output
  Data Type DINT

Example

Structured Text

(* TcpClose example *)
CASE StepCounter OF
0:
  Inst_TcpClose(TRUE, MySocketID);
  StepCounter := StepCounter + 1;
1:
  Inst_TcpClose(TRUE, MySocketID);
  IF Inst_TcpClose.Done THEN
     Inst_TcpClose(FALSE, 0);
     StepCounter := StepCounter + 1;
  END_IF;
END_CASE;