File Tools Function Blocks
This section documents function blocks that can be applied to files.
| Fucnction Block |
|
Use |
|---|---|---|
| FileClose | F_CLOSE | Close an open file |
| FileCopy | F_COPY | Copy a file |
| FileDelete | F_DELETE | Remove a file |
| FileEOF | F_EOF | Test if the end of the file is reached in a file that is open for reading |
| FileExists | F_EXIST | Test if a file exists |
| FileOpenA | F_AOPEN | Create or open a file in append mode |
| FileOpenR | F_ROPEN | Open a file for reading |
| FileOpenW | F_WOPEN | Create or reset a file and open it for writing |
| FileReadBinData | FA_READ FB_READ |
Read binary data from a file |
| FileReadLine | FM_READ | Read a string value from a text file |
| FileRename | F_RENAME | Rename a file |
| FileSeek | F_SEEK | Set the current position of a file |
| FileSize | F_GETSIZE | Get the size of a file |
| FileWriteBinData | FA_WRITE FB_WRITE |
Write binary data to a file |
| FileWriteLine | FM_WRITE | Write a string value to a text file |