GANTRY.PL.ERR
GANTRY.PL.ERR is the result of AXIS1.PL.FB – AXIS2.PL.FB when GANTRY.STATE = 2.
If GANTRY.STATE is not equal to 2, then the value of GANTRY.PL.ERR will be 0.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-02-02-000 |
General Information
| Type | Read Only |
| Description | Reads the position error present when the drive is in Gantry Mode |
| Units |
Rotary: counts, rad, deg, custom units, 16-bit counts Linear: counts, mm, µm, custom units, 16-bit counts See Position Units for details. |
| Range | Depends on units. See Position Range for details. |
| Default Value | N/A |
| Data Type | Float |
| See Also | AXIS#.PL.FB |
| Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
GANTRY.PL.ERR | 0x300E:1 (position unit scaling, uses axis 1 scaling):1 | 0x4 | INT | 1:1 | - | RW | False |