GANTRY.PL.ERRFTHRESH
Description
This parameter sets the maximum position error. If the position error GANTRY.PL.ERR is larger than GANTRY.PL.ERRFTHRESH then the drive generates a fault. If GANTRY.PL.ERRFTHRESH is set to 0, the maximum position error is ignored.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-02-02-000 |
General Information
| Type | Read/Write |
| Description | Sets the maximum position error for Gantry Mode |
| Units |
Rotary: counts, rad, deg, custom units, 16-bit counts Linear: counts, mm, µm, custom units, 16-bit counts See Position Units for details. |
| Range | Depends on units. See Position Range for details. |
| Default Value |
42949672960 counts
|
| Data Type | Float |
| See Also | AXIS#.PL.FB |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
GANTRY.PL.ERRFTHRESH | 0x300E:2 (position unit scaling, uses axis 1 scaling) | 0x4 | INT | 1:1 | - | RW | False |