IL.FOLDWTHRESH
Description
IL
"Instruction list"
This is a low-level language and resembles assembly.FOLDWTHRESH is the warning level of the current foldback algorithm. When IL.IFOLD drops below IL.FOLDWTHRESH a warning is generated.
To ensure that the current foldback warning level is never reached, IL.FOLDWTHRESH should be set well below the continuous current value for both the drive and the motor. You can also set the IL.FOLDFTHRESH value to zero.
General Information
|
Type |
NV Parameter |
|
Units |
Arms |
|
Range |
0 to 500 Arms |
|
Default Value |
0 A |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/0 |
M_01-00-00-000 |
Related Topics