IL.KPLOOKUPVALUES

Description

Retrieves the Current Loop Gain Scheduling Table in a comma delimited table.

This table is 256 records long, and the table will return values in the following format:

-->ILClosed"Instruction list" This is a low-level language and resembles assembly.KPLOOKUPVALUES

Index Value

0, 100.000

1, 100.000

2, 100.000

3, 100.000

4, 100.000

5, 100.000

6, 100.000

7, 100.000

8, 100.000

9, 100.000

10, 100.000

General Information

Type

R/W Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Table

See Also

IL.KPLOOKUPINDEX, IL.KPLOOKUPVALUE, IL.KP

Start Version

M_01-04-00-000

Related Topics

Current Loop