FunctionMLCNVConnect

Description

Connect a converter Pipe Block to the specified axis. When using the Pipe Network for coordinated motion, Pipe Blocks have to be Activated, Connected, and then Powered On before move commands work.

The Converter block changes the incoming flow of values to continuous position output with no periodicity. If a converter block is not connected to an Axis, it does not send position output values to its assigned Axis. Every pipe branch must end in a converter, whether or not it is connected to a destination Axis object, as seen in Figure 1 below.

MLCNVConnect

Figure 7-93: MLCNVConnect


  • All converters in the Pipe Network can be connected at once with the command PipeNetwork(MLPN_Connect). This calls automatically generated code with MLCNVConnect commands for each Converter block. Therefore, in a multi-axis program only one command can be used to connect Pipe Blocks instead of writing code for each Axis separately.


  • The converter block has the ability to control the analog output on the AKD. See for information on the parameters.

Arguments

Input

BlockID Description ID number of an initiated Converter object
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit N/A
  Default
AxisID Description ID number of an initiated Axis object
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit N/A
  Default

Output

Default (.Q)

Description Returns TRUE if the converter is connected to the Axis object

See more details here.

  Data type BOOL
  Unit N/A

Return Type

BOOL

Related Functions

MLCNVConnectEx

MLCNVDisconnect

MLCNVInit

Example

Structured Text

//Connect a converter Pipe Block named “CNV1”  to Pipe Block AXIS1
MLCNVConnect( PipeNetwork.CNV1, AXIS1 );

Ladder Diagram

MLCNVConnect: LD example

 

Function Block Diagram

MLCNVConnect: FBD example

Go back to the top of the page [Top]